Tecnomatix
Manipulate Location in Path Editor has no impact on final result
2021-10-07T00:01:57Z
Virtual RealityProcess Simulate
Summary
Details
When going to Manipulate Location, the Position is corrected and everything looks fine, but when trying to run, the motion is the same as before the change.
Solution
Use the Clear Teach Location command from the Robot menu in the ribbon. This removes the taught location. The Robot Configuration can also be removed as well, if desired.
Notes and References
Hardware/Software Configuration
Platform: na OS: windows OS Version: 1064 Product: TECNOMATIX Application: PROCESS_SIMULAT Function: APPLICATIONS