Failed to connect to Excel events while launching Excel spreadsheet from NX

2021-10-06T23:27:54Z

Summary


Details

Failed to connect to Excel events while launching Excel spreadsheet from NX

Solution

In Windows registry there are two entries which is causing this problem

In HKEY_CLASSES_ROOT, search for this class ID D99CD578-9510-4014-9161-F01778698159,
 Under InprocServer32 , two entries are listed.

If the user runs unregister_splm_files.bat, only one entry is getting removed.  
Manually remove the other entry and run register_splm_files.bat.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V1953
Function: SPREADSHEET

Ref: 002-8529354

KB Article ID# PL8529354

Contents

SummaryDetails

Associated Components