Sample TDP template import is failing with error "Failed to initialize import operation" "Error:941448".
2021-10-06T23:27:54Z
Summary
Details
While trying to import sample Technical Data Package Template (TDP) to Teamcenter using the OOTB command-line utility, the import is failing with the error "Failed to initialize import operation" "Error:941448".
Solution
Verify if FMS_HOME has been set correctly while executing the command.
Check if the fcc is running?
After setting the FMS_HOME mostly the issue will not occur.
Notes and References
9981793
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: TECH_DATA_PKG Version: V1953 Function: TEMPLATE