RobotExpert Controllers for ABB, CLOOS, COMAU, DEFAULT, DENSO, EPSON, FANUC, HHI, IGM, KAWASAKI, KUKA, MITSUBISHI, NACHI, NC, PANASONIC, STAUBLI, TOOLS/OLP_TOOL, UNIVERSAL, YASKAWA

2021-10-07T00:16:52Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that RobotExpert controllers for "ABB, CLOOS, COMAU, DEFAULT, DENSO, EPSON, FANUC, HHI, IGM, KAWASAKI, KUKA, MITSUBISHI, NACHI, NC, PANASONIC, STAUBLI, TOOLS/OLP_TOOL, UNIVERSAL, YASKAWA" are available for download from https://support.sw.siemens.com.

   See RobotExpert_Controller_Name_changes_log.htm for details concerning this update.
   Note: This file is located in the 'OLP Change Logs' folder directly under the
              'RobotExpert Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
   - Scroll down and toggle On the Tecnomatix product.
   - Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'RobotExpert Robot Controllers'
- Select 16.1

Download the file(s):

    RobotExpert_16.1_ABB_RAPID_64BIT_v3.66.6_05_03_2021.exe
    RobotExpert_16.1_CLOOS_CAROLA_64BIT_v2.21_27_01_2021.exe
    RobotExpert_16.1_COMAU_PDL_64BIT_v4.9.7_28_01_2021.exe
    RobotExpert_16.1_DEFAULT_64BIT_v2.79_17_03_2021.exe
    RobotExpert_16.1_DENSO_PACSCRIPT_64BIT_v2.26_17_03_2021.exe
    RobotExpert_16.1_EPSON_SPEL_64BIT_v2.13_27_01_2021.exe
    RobotExpert_16.1_FANUC_RJ_64BIT_v3.9_17_03_2021.exe
    RobotExpert_16.1_HHI_HRBASIC_64BIT_v1.2_27_01_2021.exe
    RobotExpert_16.1_IGM_INS_64BIT_v1.42_27_01_2021.exe
    RobotExpert_16.1_KAWASAKI_AS_64BIT_v4.12_10_03_2021.exe
    RobotExpert_16.1_KUKA_KRC_64BIT_v4.39.1_17_03_2021.exe
    RobotExpert_16.1_MITSUBISHI_MELFA_64BIT_v0.17_27_01_2021.exe
    RobotExpert_16.1_NACHI_SLIM_64BIT_v4.27.2_05_03_2021.exe
    RobotExpert_16.1_NC_CODE_64BIT_v2.6.12_12_03_2021.exe
    RobotExpert_16.1_OLP_TOOL_64BIT_v15.8_20_02_2021.exe
    RobotExpert_16.1_PANASONIC_CSR_64BIT_v2.16_27_01_2021.exe
    RobotExpert_16.1_STAUBLI_VAL_64BIT_v3.13_27_01_2021.exe
    RobotExpert_16.1_UNIVERSAL_URSCRIPT_64BIT_v3.19_27_01_2021.exe
    RobotExpert_16.1_YASKAWA_INFORM_64BIT_v5.18.2_10_03_2021.exe


To Install:

Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the RobotExpert installation).

Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software



SFB-TECNOMATIX-8529140
Product Information:
  • Product: TECNOMATIX , Application: ROBOTEXPERT , Version: V16.1

KB Article ID# PL8529140

Contents

SummaryDetails

Associated Components