NX In TC IMM how we can add release status " Full released/conditional released/Obsolete/Rejected/Any" to material revision?

2021-10-06T23:27:54Z
NX for Design

Summary


Details

In IMM how we can add release status " Full released/conditional released/Obsolete/Rejected/Any" to material revision?
 
When we search material when we invoke IMM within NX we could see the material status as Full released/conditional released/Obsolete/Rejected/Any. Can we set only a unique value in this field like we want users to always search fully released materials and not obsolete or any then how can this be achieved?
 
In Teamcenter IMM how we can add the release status mentioned above " Full released/conditional released/Obsolete/Rejected/Any" to material revision.


Solution

If you want to add/remove the statuses and change the Display or Real name of the statuses then check the Teamcenter Preferences "IMM_TC_Display_Statuses" and "IMM_NX_Display_Statuses".


There you can add remove statuses and changes the display or the real name of the statuses. Refer to the below snapshot of the Teamcenter preferences-


KB Article ID# PL8529134

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX