Best practices while using JT file in NX Drafting Application.

2021-10-06T23:27:54Z

Summary


Details

Sometimes user-facing issues while working in drafting and creating views while using JT in  NX drafting application. Users can reduce or avoid the upcoming issue of drafting through best practice.

1. View update issue.
2. View creation issue.
3. Internal error.
4. View Edit issue.     etc...

Solution

Best practices:



1. Open the file in NX.


2. Do Examine Geometry:


This command analyzes a solid body, face, or edge for conditions of interest (for example, tiny objects, problems in the data structure, self-intersections, and spikes/cuts).


Regular use is allowing model integrity to be maintained, reducing potential issues caused by invalid geometry.


3.Part Cleanup:


The Part Cleanup command eliminates certain objects from the part file. Without Part Cleanup, these objects are inaccessible, and cannot be eliminated.


 


The options are grouped according to their effect on the data:


 


a. Simple Cleanup Actions are safe operations in that they do not change data.


 


b. Moderate Cleanup Actions generally change the data in ways that deserve to be changed. However, there is some risk that their application will execute changes that you do not intend.


 


c. Serious Deletion Actions (Use Caution) perform higher-risk operations in that they always remove data.


4. Optimize Face:


Use the Optimize Face command to simplify surface types, merge faces, improve edge accuracy, and recognize blends.


5. Examine Geometry:


Note: If still, JT can't pass examine geometry, please correct part files and recreate JT to avoid the upcoming issues in drafting application.



Notes and References

10011132 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW

Ref: 002-8529133

KB Article ID# PL8529133

Contents

SummaryDetails

Associated Components