Solid Edge certified on Windows 10 LTSC/LTSB?

2021-10-06T23:58:18Z

Summary


Details

Is Solid Edge certified on Windows 10 Long-Term Servicing Channel (LTSC)  or Long-term Servicing Branch (LTSB)?

Solution

We do not test with Windows 10 LTSC or LTSB Versions and consequently the Long-Term Servicing Channel/Long-term Servicing Branch release is not a certified operating system for Solid Edge.

Please check the Solid Edge Readme text file for the certified requirements. The file can be found on Support Center in the main Solid Edge Download or in the Solid Edge Installation folder.

Theoretically, based on the the Microsoft Support and Update terminology, the customer would need to test the target Solid Edge version plus Maintenance Pack on the LTSC/LTSB machine and then NOT apply any more Solid Edge updates. Customers will have to evaluate each Solid Edge major release & Maintenance Pack for suitability with LTSC/LTSB and freeze on that combination.




Notes and References

LTSC (Long-Term Servicing Channel) previously called LTSB (Long Term Servicing Branch) 

Important: The LTSC release is intended for special use devices. Support for LTSC by apps and tools that are designed for the semi-annual channel release of Windows 10 might be limited.

Detailed Information about this Servicing Type can be found following the links to the Microsoft Documentation:

https://docs.microsoft.com/en-us/windows/whats-new/ltsc/

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V221.0
Function: INSTALL

Ref: 002-8529132

KB Article ID# PL8529132

Contents

SummaryDetails

Associated Components