Solution for extracted edges from model in drafting view isn't smooth.

2021-10-06T23:27:54Z

Summary


Details

As per the default resolution tolerance settings curve value is set 0.005 in NX. For small and ellipse curves predefined tolerance settings do not provide desired display results.


Refer to the below image as an example: Radial dimension 0.15, does not display smooth.


Solution


Set Default Curve value as 0.001 from 


Menu>Preferences>Visualization>Preference>Accuracy>advanced>curve.


See the below image, curves are displayed smoothly.

Note:


The finer tolerance settings can increase memory consumption and reduce display performance.



Notes and References

IR 10012258 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1926
Function: DRAWING/VIEW

Ref: 002-8529131

KB Article ID# PL8529131

Contents

SummaryDetails

Associated Components