Solid Edge 2021 - Maintenance Pack 4 Announcement

2021-10-07T00:10:06Z

Summary


Details

March 22, 2021
 
Dear Solid Edge Customer: 
 
Solid Edge 2021 Maintenance Pack 4 is now available for download.
 
We appreciate your continued business and your participation in the software support process - - your reporting helps us make Solid Edge more productive for the way you do business.
 
Sincerely,
The Solid Edge Team 
 
============
Release Notes:
============
 
Solid Edge 2021 MP4
Version: 221.00.04.03
 
Solid Edge 2021 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
 
Solid Edge 2021 Maintenance Pack download area on Support Center:
 
https://support.sw.siemens.com/product/246738425/downloads
 
===============
E-mail Notification: 
===============
 
Plug-in to the electronic advantage by subscribing to our e-mail distribution services. This service keeps you informed of pertinent technical information automatically and in a timely manner using electronic mail. To receive direct e-mail notifications for Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
 
   https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
============================================
This Maintenance Pack addresses the following PRs:
============================================
 
===General===
PR 8465041: Periods replaced with commas when adding/editing property value
PR 9588911: Export of .3mf on 3D-Print after reorient does not work
PR 9875781: Material context menu opens delayed if Material Table Folder uses a UNC Path
PR 9973105: Cannot disable Upload to YouTube via Options.xml file 
PR 9981499: 3Dfind.it searching for similar models in shape
PR 9981978: Not all the dialogs interpret the propseed.txt the same way
PR 9989872: Cannot generate XML of broken links because not permitted to use a style sheet
PR 9987643: Error in Licensing: Piping Design Add-On and Foundation
PR 9994251: 'go-to' in Simulation geometry environment broken in MP
PR 9992538: Unable to disable Share PDM Log files
PR 10005735: REG_DWORD "Enable Teamcenter Share" set to 0 does not work
 
===API===
PR 9985000: Wrong tooltips on the main toolbar when using SolidEdge API function
PR 9982710: API retrieves incorrect bend angle in a given sheet metal part  
 
===Assembly===
PR 9974531: Pathfinder blocked by the invisible box
PR 9984086: Solid Edge is crashing
PR 9468973: Constraints in the top-level assembly are failed after making a sub as adjustable
PR 9985115: Unable to get Enclosure feature value
PR 9988357: Issue in editing path of wire in electrical routing
PR 9986196: Bundle issues with Route along Surface at Electrical Routing
PR 9998078: Solid Edge Crashes when opening this subassembly
PR 9975718: The TOP assembly disappeared in [Pack and Go]
 
===Draft===
PR 9973808: Dimensioning in an isometric Detailed View is incorrect
 
===Part/Profile/Sheetmetal===
PR 9904892: Unable to get Enclosure feature value
PR 9951808: 2D Nesting and German variable names.
PR 9993303: Crash when moving faces in the assembly environment
PR 9934203: Rigid Set violated by Auto-scale Sketch command
 
===Teamcenter Integration for Solid Edge===
PR 9868929: Save As on OOD assembly and the user has to dismiss the same message many times
PR 9988713: Revise do not copy the existing revision description
PR 9992830: cannot Ctrl V to paste into the SE Teamcenter parts library search field
PR 9995727: Project IDs are lost in Solid Edge while Hide CPD is on and part window closed
PR 9999217: Parts and subassemblies are being Checked Out automatically, despite SE Options
PR 10000336: Title block does not update when a draft is opened
 
===Solid Edge Data Management===
PR 9947390: SEDM open drawing doesn't work
PR 9956197: SEDM open Drawing returns a list including assemblies
PR 9869083: SEDM hangs up when creating a new revision
 
===Translators===
PR 8452437: Unable to create multi-edge flange in this case
PR 9858402: Inventor Migration relationships not coming through
PR 9963467: Inventor to Solid Edge Issues - migration terminated
PR 9971136: Bad IFC Translation
PR 9604743: Cannot open two specific PRO-E Part documents (created with CREO Elements 3.0)
PR 9958684: Inventor Migration failed
PR 80610: Edge/surface association of PMI dimensions is not working in NX1980.1100
 
===TechPub===
PR 9947386: 3D Publishing - Group animation in HTML
PR 9951961: 3D Publishing - Scrollbar automatically goes up
PR 9952919: 3D Publishing - Part list highlight in HTML
PR 9972776: Carousel incorrect display in HTML
PR 9980492: Updating using Solid Edge assembly brings in extra parts in exploded steps
 

SFB-SOLID_EDGE-8529026
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8529026

Contents

SummaryDetails

Associated Components