The value removed from Property manager remains in the Check In CPD
Solution
When property value removed from property manager and sent it to checkin value will be shown in CPD due to "SEEC_Property_Sync_PDM_Master" which is used to sync the file when file is uploaded.
This is working as designed.
Hence properties will show in property manager when assign values in CPD.
To not to see some unnecessary properties then remove them from CPD and upload/Check-in the file.
After check-in these removed property values will not show any values in property manager .
Notes and References
10005128Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC
Ref: 002-8528993