Configure client with different license servers for Solid Edge and Teamcenter

2024-08-05T04:18:57Z

Summary


Details

Is it possible to configure the client to point to different floating license servers such that Solid Edge/SEEC is hosted on one license server and Teamcenter is hosted on a different license server?

Solution

Yes, this is technically possible.

 

Teamcenter uses the environment variable SPLM_LICENSE_SERVER to define the location of

the FlexLM Server.

Since Solid Edge 2020, Solid Edge uses the environment variable SE_LICENSE_SERVER.

Defining these two environment variables differently will allow the licenses to be checked out from different license servers e.g.

Control Panel > System > Advanced System Settings > Environment Variables > System Variables:

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8528740

Contents

SummaryDetails

Associated Components