NX Save As dialog result differs based on the selection of assembly in the Assembly Navigator

2021-10-06T23:27:54Z
NX for Design

Summary


Details

Save As dialog result differs based on the selection of assembly in the Assembly Navigator

If the assembly is selected and performs Save As, The dialog is displayed as follows


If the assembly is not selected in assembly navigator, the following dialog is displayed


Solution

If the assembly is selected in the ANT, NX gives option to select Part from the loaded parts for the save as operation, but if the assembly is not selected in the ANT, then only the top assembly can be performed save as operation.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1926
Function: FILE_SAVE_AS

Ref: 002-8528731

KB Article ID# PL8528731

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX