Details
Custom item revision attribute value mapped on UGPART dataset is locked
Have mapped the Item revision attribute on UGPART dataset. Want to set attribute value in NX which should reflect in Teamcenter Item revision object.
Solution
It is not possible to synchronize attributes on a UGPART to an Item Revision Master because the Item Revision can have multiple UGPART datasets which makes conflicts.
Whereas Item Revision should have only one UGMASTER and can be mapped with Custom item revision attribute value.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1926
Function: ATTRIBUTES
Ref: 002-8528730