NX What is Administration logging and Security Logging in Teamcenter Integration Preferences?

2021-10-06T23:27:54Z
NX for Design

Summary


Details

What is Administration logging and Security Logging in Teamcenter Integration Preferences?



Solution

Administration Logging - This option is available only if you have administrator privileges.
This enables the creation of administration log files. The administration.log file lists the Teamcenter system administration objects (for example, users, groups, volumes) that were created, modified, deleted, or released.



 Security Logging  - This option is available only if you have administrator privileges.
 This enables the creation of security log files. The security.log file lists the users who performed protection violations. For example, users who attempted to open a dataset without read access).
 
 These file locations are defined by the %TC_LOG% environment variable location, which by default is located at: 
  %TC_DATA%\log_%TC_DB_SERVER%_%ORACLE_SID%



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1926
Function: PREFERENCES

Ref: 002-8528607

KB Article ID# PL8528607

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX