Where "Set NX Default Folder" setting is stored in AWC environment?

2021-10-06T23:27:54Z

Summary


Details

Set any folder as "Default Folder" with "Set NX Default Folder" command in the Active workspace tab, some NX sessions doesn't update in File Open dialog

Where "Set NX Default Folder" setting is stored?




Duplication Steps


1.   Go to Active Workspace tab in NX.


2.   Select any folder and set as default folder using "Set NX Default Folder"


3. File -> Open



In File Open dialog "Default Folder" doesn't point to the folder set using "Set NX Default Folder"



Solution

Set Default Folder is a equivalent to setting Default Folder in TC  navigator. This is the default Folder in which New Parts that are created will be placed.

This setting gets stored in HKEY_CURRENT_USER\software\unigraphics solutions \NX\12.0\General\UGManager\DefaultContainer

If file open last look-in is not stored in registry, then NX will default to the "Default container"  set using "Set NX Default Folder".

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 002-8528606

KB Article ID# PL8528606

Contents

SummaryDetails

Associated Components