Check-Mate window does not activate even if "View Check-Mate Result" function executes.
2021-10-06T23:27:54Z
Summary
Details
Even if "View Check-Mate Results" or "Execute Current Tests" executes, the result window does not come up and the result cannot be confirmed.
Steps to reproduce: 1. open any part and put a box solid. 2. go to "HD3D Tools" tab and "Execute Check-Mate Tests" with any chosen checkers such as "Examine Geometry". *** You should find the result of passed/failed. 3. go to PNT or other tabs. 4. "Tools" > "View Check-Mate Results". *** The window will not be activated and you cannot see any result. 5. "Tools" > "Execute Current Tests". ***It's the same as well(, but In graphic window shows the result of Failed.)
There is no problem at first time to make function executed, but the issue occurs at second time or later. In addition, it's not solved even if the part is closed and reopened, but it's solved by restarting NX.
Solution
The issue is fixed in NX1969.
Workarounds: one of following When click "View Check-Mate Result" for the second time, the Check-Mate gadget actually was activated already by the first time, so you can click the HD3D tools button on the side bar to view it. or you can de-active the Check-Mate gadget explicitly before leaving HD3D Check-Mate environment, then when you execute the function, it will activate and show the Check-Mate gadget again.
Notes and References
It's the issue only in NX1953 Series(1953, 1957, 1961 and 1965).
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: KDA Version: V1953 Function: VALIDATION