Solid Edge Windows 10 Update (K5000802) - Print issues in Solid Edge - Resolved

2021-10-07T00:10:06Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

The Microsoft March 9, 2021 Update, also known as KB5000802, introduced print-related issues in Solid Edge. A quick Google search for KB5000802 will provide an indication of how disruptive the KB5000802 Windows 10 update has been. If non-enterprise customers do not have the Windows 10 automatic update delay set, the KB5000802 update has most likely downloaded and installed automatically on your machines. 
 
Thus far the impact to Solid Edge has been limited to missing data when creating PDF files, primarily loss of shaded views. There have been multiple reports from customers running Solid Edge ST10, Solid Edge 2019, and Solid Edge 2021. So, it would appear that any version of Solid Edge could be subject to printing problems as a result of the Windows 10 KB5000802 update. 
 
Based on the increasing level of negative chatter being posted on the various Windows 10 forums, hopefully, Microsoft will address the issue very soon. For now, the only way to resolve the print-related issues in Solid Edge is to uninstall the KB5000802 update.
 
We have opened a tracking PR for the March 9, 2021, KB5000802 update. If you are experiencing this type of printing problem, contact your Partner and asked to have an IR opened on your behalf to be appended to PR#10011002. Or if you are a direct customer, open an IR on Support Center or call your local Siemens Customer Support number and make a request to be appended to PR#10011002. Once Microsoft has resolved the problem, we will set the status of the PR to resolved and you will then be notified via the Customer Response letter process.

Update:
3/18/2021 - Microsoft has resolved the issue in update KB5001649.

https://docs.microsoft.com/en-us/windows/release-health/status-windows-10-2004#1573msgdesc

Resolution: This issue was resolved in the out-of-band update  KB5001649. It is a cumulative update, so you do not need to apply any previous update before installing it. You will need to Check for updates to install KB5001649 and might need to also select Download and Install. For instructions on how to Check for updates, please see Update Windows 10. You can import this update into Windows Server Update Services (WSUS) manually. See the Microsoft Update Catalog for instructions.


Note KB5001649 is cumulative and addresses both the issue above and the issue addressed in the March 15, 2021 out-of-band release for the APC_INDEX_MISMATCH error with a blue screen.




SFB-SOLID_EDGE-8528069
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8528069

Contents

SummaryDetails

Associated Components

SE_BETA