Problem in Simcenter 3D Specialist Durability in calculating the static safety factor in the strain-life approach

2021-10-07T00:09:09Z

Summary


Details


In Simcenter 3D Specialist Durability, the static safety factor is calculated by comparing the max stress with the tensile strength and the min stress with the negative compressive stress.
 
 An issue was detected in the strain-life analysis, where the role of the tensile and the compressive strength have been interchanged when calculating the static safety factor. So in the case both values are different the static safety factor is wrong


As a workaround to  calculate the correct static fatigue safety factor, one can exchange the values of compressive and tensile strength in the material data. Be aware that this can have influence on the damage evaluation as well


Problems are solved in Simcenter 3D 2021.1-1969. 

SFB-NX-8528068
PR 9996211
Product Information:
  • Product: NX , Application: CAE , Version: V1926

KB Article ID# PL8528068

Contents

SummaryDetails

Associated Components