Open in Solid Edge not working when dataset has no named reference

2021-10-06T23:58:16Z

Summary


Details

The customer provided this workflow that will result in an error in Solid Edge

In the RAC: 


  • Create new Item
  • Create a Solid Edge Part dataset for Item Revision, do not import any SE file. 
  • Open the new Solid Edge Part from RAC with "Open in Solid Edge" 
You will see now the following three messages in Solid Edge and no file  is opened:
 
 
 

 


Why does this happen?
 
 

Solution

This is working as designed. 

When the dataset is created we expect there must be a Solid Edge file associated with it.

If you delete the dataset and try opening the empty item revision, Solid Edge will ask you to select a template. It will create a Solid Edge dataset with named reference and open the empty file.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 002-8528061

KB Article ID# PL8528061

Contents

SummaryDetails

Associated Components