How to create a dual dimension using the Measure command

2021-10-06T23:27:54Z

Summary


Details

How to create a dual dimension using the Measure command 



Solution

1. With the Measure command dialog open, enable the Display Annotation option.
2. After the annotation/dimension has been generated, click OK in the Measure dialog.
3. MouseButton3 on the dimension and select 'Settings'. 
4. In the left column of the dialog, highlight 'Dual' and enable the option 'Show Dual Dimension'.


Note: The PMI Module must be enabled for this to work. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1919
Function: ANALYSIS_REQUES

Ref: 001-10011271

KB Article ID# PL8527908

Contents

SummaryDetails

Associated Components