Connection Failed ...

2021-10-06T23:58:15Z

Summary


Details

When attempting to connect to Electrical Manager an error message is displayed ...


Connection Failed


Could not connect to Solid Edge Electrical Manager.  Application Terminated.



Solution

This issue can result from several different root causes.


On the Client workstation ...


  • See if the client can reach the server.
    • Open up a Command Prompt, using the 'ping' command, ping the server.
  • Insure that the clientprops.xml file is pointing to the correct server name or IP address.
On the Server ...


  • Insure that the Electrical Manager and Database services are running
    • Electrical Manager process is running
    • PostgreSQL Server processes are running
  • Within the managerprops.xml file, insure that the iorconnection statement specifies "remote" and not "local"
  • Insure that there are no firewall settings that block TCP/IP traffic on the client or server.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Function: OTHER

Ref: 002-8527887

KB Article ID# PL8527887

Contents

SummaryDetails

Associated Components