Synchronizing Structure Manager "Usage Address" and "Position Designator" attributes with NX.

2021-10-06T23:27:54Z

Summary


Details

BomLine attribute "bl_ref_designator"  (Display Name: Reference Designator) can be synchronized between Teamcenter structure manager and NX using occurrence notes.
Please refer to the documentation below.

https://support.sw.siemens.com/en-US/product/209349590/knowledge-base/PL8002232?pid=sc%3Asearch&pid_context=reference%20designator&index=content-external&audience=external

The user wants to synchronize attributes "bl_usage_address" and "bl_position_designator" between the Structure manager and NX.

Solution

This mapping is only for the Reference Designator property on BomLine (bl_ref_designator)
Note: It cannot be scaled to any and every property.

The user has to create his own customized occurrence notes for "Usage Address" and "Position Designator"  to sync them between the Structure manager and NX.
Please refer to the documentation below.

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&p=1&q=001-9808705&file_type=html&i=001-9808705&k=0&o=0



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1953
Function: ATTRIBUTES

Ref: 002-8527880

KB Article ID# PL8527880

Contents

SummaryDetails

Associated Components