ugto2d utility not working in managed NX

2021-10-06T23:27:53Z

Summary


Details

Running the dxfdwg command line translator fails with the message: 
Invalid arguments - No input parts to process 
or the message: 
inavlid extension provided - cannot translate 
  
     *notice this message is spelled wrong and should read: invalid extension provided - cannot translate


Running the command line in managed mode with the following input: 
dxfdwg.exe -pim=yes -u=infodba -p=infodba -g=dba -i=@DB/testpart/01/specification/testpart-dwg1 -o=c:\temp\testpart.dxf -d=C:\temp\dxfdwg.def 



Solution

The issue is that the last arguments do not have a dash (-) in front of them. 
Usage : dxfdwg i=<inputfile> o=<outputfile> l=<logfile> d=<deffile>


Try this input instead without the dashes in front of the utility arguments for i, o, l, and d: 
dxfdwg.exe -pim=yes -u=infodba -p=infodba -g=dba i=@DB/testpart/01/specification/testpart-dwg1 o=c:\temp\testpart.dxf d=C:\temp\dxfdwg.def 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1926
Function: UTILITIES

Ref: 001-10003075

KB Article ID# PL8527791

Contents

SummaryDetails

Associated Components