Error message when translating a file to dxf or step to unmanaged drive.

2021-10-06T23:58:12Z

Summary


Details

Receiving a Teamcenter Popup message when translating a managed file such as dxf or step to disk (unmanaged). Dismissing the informational dialog box continues  the translation as expected.



Solution

There are 2 places in the Solid Edge User Interface that can trigger this informational Pop-Up box. The first is located in Solid Edge Options (Application Button -> Settings -> Options) under the Manage ->General tab. 

"Save Translation to Teamcenter" 

By checking the box, "Enable Save Translation to Teamcenter" you are instructing SEEC to evaluate the SEEC preference in Teamcenter, SEEC_Save_Translation. 

This preference provides multiple options on save methods, naming conventions, etc. for managed saved translations. However, if the preference has NOT been configured AND the Option setting discussed above is checked, then you get the Teamcenter (SEEC) Informational Pop-up box describing the current condition of your local Solid Edge settings.


The second location for this toggle is also controllable in the Solid Edge UI. Under the Teamcenter Menu is a button, Save Translation to Teamcenter. When pressed it sets the option as discussed above to "checked" and the button's background should be light blue. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1903
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 001-10005732

KB Article ID# PL8527750

Contents

SummaryDetails

Associated Components