Reference sets translated from NX to JT are not working as expected. When the JT is viewed, it doesn't match the view from NX. It's showing another formation of the same part, and misplaced.
Solution
This is due to the user not properly utilizing the "useRefSets" option in the tessUG.config file.
In this case, the user set useRefsets = "MODEL" which only translated the MODEL reference set. The reference set needed was "HARNESS2". Changing "useRefsets = "ALL" resolved this issue. Then the user was able to change the reference set in TcVis to HARNESS2 to see the proper formation of the part in the correct location.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V1892
Function: NX_JT
Ref: 001-9999178