Details
A Draft Table continuous Text is displayed differently in Solid Edge installed on Windows 10 than on Windows 7 where the Text was originally created.
Solution
The reason for this is that Microsoft changed Fonts with Windows 10.
To resolve the user needs either to modify the text style in Solid Edge e.g. editing character distance or removing the installed font and installing the original Windows 7 Font.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V221MP3
Function: TABLES
Ref: 002-8527555