NX Copy/Paste FCF and edit, the copy source will also change.

2021-10-06T23:27:53Z
NX for Design

Summary


Details

Copy/Paste FCF and edit, the copy source will also change

There is a difference in the behavior on where the Copy operation is performed.

1. Copy/Paste on-screen:

2. Copy/Paste done in Part Navigator:




Solution

When doing copy/paste from the PMI node in the part navigator, you are creating a new PMI object. Note that there is a new entry under PMI.


When you pick from the screen (or from the PMI display instances listed within the model views in the navigator), you are making a new instance of the same PMI. As an instance of the same PMI, the changes in one instance will be displayed in any others. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1909
Product: NX
Application: PMI
Version: V1934
Function: FCF

Ref: 001-9993180

KB Article ID# PL8527455

Contents

SummaryDetails

Associated Components

PMI