Solid Edge Show/Hide of Sub-Assemblies "freezes" Solid Edge for a long period

2021-10-06T23:58:11Z
ASSEMBLY

Summary


Details

In this scenario, after upgrading from Solid Edge 2020 to Solid Edge 2021, the user finds they are waiting for a long period every time they show/hide a subassembly.

Their main assembly was opened in "Large Assembly mode", with all parts hidden, so making some subassemblies visible is taking many minutes.
  

Solution

In this instance, the user forgot to exclude all ".asm" file types from Virus Scan, so showing a subassembly resulted in several Gigabytes of network transfer instead of some hundred Kilobytes without Virus Scan.

By adding ".asm" files to the exclusion list in the virus scanner solved the problem.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Function: DISPLAY

Ref: 002-8527438

KB Article ID# PL8527438

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS