NX How to modify the value of "mom_kin_rapid_feed_rate" inside of NX Post Builder

2021-10-06T23:27:53Z
NX for Manufacturing

Summary


Details

User has manually changed value of the "mom_kin_rapid_feed_rate" variable by directly modifying the tcl file of the post file set.  Can this value be set inside Post Builder, rather than by text editor?

Solution

Hand edits of the post builder files are not recommended.  The rapid traversal rate is a property of the machine tool definition in the post.  On the Machine Tool tab, go to the General Parameters.  On the right side of the page, there will be a Traversal Feed Rate field to set this kinematic value in the UI:



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1899
Function: POSTBUILDER

Ref: 002-8527192

KB Article ID# PL8527192

Contents

SummaryDetails

Associated Components

Manufacturing Post Builder