When executing Drawing Update after creating a cross hatch, "Out of Date(!)" flag is raised.
2021-10-06T23:27:53Z
Summary
Details
Description: If "Boundary curves" is selected as "Selection mode" in "Crosshatch" function and the crosshatch is created, "Out of Date(!)" flag is raised on the part file window tab after executing "Drawing Update" function even though "Delay Link Update" is turned off.
The condition to be reproduced: If all the conditions are met, the problem occurs 1. In case of loading a part is "Partially Load", "Partially Loaded - Lightweight Display" or "Minimally Load - Lightweight Display". 2. Drawing View condition is "Exact (Pre-NX8.5)" and "Extracted Edges" is not used. 3. Crosshatch target geometry: Exists in the external part (in other component part), not in the work part. Under the condition above, the phenomenon occurs even though "Delay Link Update" is turned off.
Step to reproduce: 1.Open the part 2.Create a crosshatch 3."Update" the drawing sheet or the view
Solution
The issue is fixed in NX 1926.
Workarounds: Executes one of following 1. When generating a crosshatch, don't use "boundary curve" (use "point in area") as "Selection Mode" 2. Use "Fully Load" or "Fully Load - Lightweight Display" as the part load option 3. If you would like to use "Exact (Pre-NX8.5)", use "Extracted Edge" 4. Delete "Exact (Pre-NX8.5)" drawing view and recreate new drawing view from scratch 5. After occurring the phenomenon, manually update the drawing by Tools > Update > Interpart Update > "Update Links" or "Update All"
Notes and References
The issue occurs only in NX 1899 Series.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DESIGN Version: V1903 Function: SELECT_INTENT