Solid Edge Using SEEC_Synchronize_ItemNumbers to Synchronize Find Number and Item Number between Solid Edge and Teamcenter

2021-10-06T23:58:10Z
DOC_MANAGEMENT

Summary


Details

How do I synchronize the Teamcenter Find Number with the Solid Edge Item Number? 

Solution

Configuration Teamcenter

Synchronization between the Solid Edge Item Number and Teamcenter Find Number can be accomplished by using two Teamcenter preferences:
 
  • SEEC_BOM_Synchronize =TRUE
  • SEEC_Synchronize_ItemNumbers = TRUE

The synchronization is between Teamcenter and the Sold Edge Assembly occurrences. When the Item numbers are required on the Solid Edge draft an additional setting on the parts list properties is needed to use the assembly generated Item Numbers

Configuration Solid Edge (Parts List drawing)
The behavior of the Item synchronization is controlled by the switches of the preference SEEC_Synchronize_ItemNumbers. This preference controls all settings on the Solid Edge Options form for the Item Numbers. (On an assembly Application -> Settings-> Options -> Item Numbers)

SEEC_Synchronize_ItemNumbers = TRUE will switch-on the "Maintain item Numbers"
/Method= (value 1-4) will control the level of synchronization where:

Method=1 is the Top Level only
Method=2 is Atomic – top down
Method=3 is Exploded – top down
Method=4 is Exploded – Use Level base numbers


The other parameters are used to control the numbering, uniqueness and weldments.


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 002-8527000

KB Article ID# PL8527000

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC