Details
Unable to select point for smart dimension
Solution
Smart Dimension command used to place a dimension on any single element, between any two elements, or between elements on a sketch, a drawing, or a model. The dimension types that are available depend on the elements you select. Since if tried to select point only there is no dimension to show for this single element. Hence user cannot select point for smart dimension as a first element.
He can select this as second element.
For example, create a line and a point. Now select smart dimension then select line and then you can select point.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V221.0
Function: DIMENSIONS
Ref: 002-8526993