Details
Output from 'SEEC_Save_Translation' and unmanaged 'Save as Flat' is different.
Solution
Sesmf.ini file is used to export flat pattern to .dxf.
Default Sesmf.ini used for 'Save as Flat' is located at '\Solid Edge <version>\Preferences\Translators' while for managed 'SEEC_Save_Translation' the ini file is used from
'\Solid Edge 2020\Preferences\Translators\SEEC'.
If there is difference in settings of these two files it will result in different output.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP10
Function: SEEC
Ref: 002-8526895