The FlexLM Options File is not read

2021-10-06T23:27:53Z

Summary


Details

The options file specified on the VENDOR line, in the license file, is not found. 
This is indicated by the following entry in the license server log file (splm_ugslmd.log):


=== Vendor Daemon ===
 Vendor daemon: ugslmd
...
=== Startup/Restart Info ===
Options file used: None



Solution

If an options file (and/or a port number) are added to the VENDOR line in the license file, the keywords OPTIONS and PORT, must be in uppercase, or they may be ignored.

An example of the VENDOR line syntax is shown below:


SERVER LIC_SERV1 COMPOSITE=ABCDEF123456 28000
VENDOR ugslmd OPTIONS="C:\ProgramData\Siemens\ugslmd.opt" PORT=28001 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: PLATFORMS
Version: V1953
Function: FLEXLM

Ref: 001-9998630

KB Article ID# PL8526697

Contents

SummaryDetails

Associated Components