Limiting number of displayed PMI to 1000

2022-08-16T15:57:58Z

Summary


Details

When we load our large assembly into standalone TcVis and try view it we see this message:

"Limiting number of displayed PMI to 1000"

We click on OK to that message and the geometry is displayed but none of the PMI.Is there a way to show more PMI?

Solution

Yes, you can control the maximum number of PMI in TcVis with a registry key. Default installs are limited to 1000.

Open RegEdit and then HKEY_CURRENT_USER\Software\Siemens\VisView\12.3\Vis Mockup\C\PMI edit the key called PMIPrefs_MaxVisiblePMI:


You can increase this number then save your changes.

Notes

KB Article ID# PL8526686

Contents

SummaryDetails

Associated Components