Solid Edge Correct Path to Local Help Server in Solid Edge 2021

2021-10-06T23:58:08Z
PART/SHEETMETAL

Summary


Details


A customer is using a local help server in their company.  Trying to enter the documented path (http://localhost:5000/tdoc/se/221/se_help#uid:index) will not be accepted by Solid Edge.

There seems to be a mistake in the documentation.



Solution

The correct path to local help server in Solid Edge 2021 will be:

"http://localhost<your Port>/en-US/product/246738425/doc/PL20190712144607070."

Note the "." at the end of path.

Of course, there will still be the need of adaption for server name (if not installed on local machine) and language (e.g. "de-DE" for German help).



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: HELP
Version: V221.0
Function: OTHER

Ref: 002-8526669

KB Article ID# PL8526669

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES