Positioning problems in PCB Exchange for mapped components

2021-10-06T23:27:53Z

Summary


Details

Exporting Model using ECAD-Export failed to apply position change of mapped components, but non mapped components worked. 



Solution

Custom configuration files were not loaded from expected location.

Customer needed to set the System Environment Variable MAYA_PCB_ENV_DIR to the location of the custom initialization files to pick the files correctly.

The issue was solved by adding the missed variable MAYA_PCB_ENV_DIR. 

Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1903
Product: NX
Application: PRINTED_CIRCUIT
Version: V1926
Function: PCB_EXCHANGE

Ref: 001-9991184

KB Article ID# PL8526643

Contents

SummaryDetails

Associated Components