NX Selecting multiple features - Feature direction is not displayed (CAM)

2021-10-06T23:27:53Z
NX for Manufacturing

Summary


Details

In NX 1926 and NX 1953 Series, when selecting multiple features in an operation, we get no indication of the feature direction in the graphics area.

Solution

In the new Manufacturing Feature Navigator the feature coordinate systems can be switched on/off with the 'Show Feature CSYS' toggle-button. Switch this on and the direction is shown in the graphics when reversing the direction in the Feature Geometry dialog.


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1953
Function: FEATURE_BASED

Ref: 002-8526623

KB Article ID# PL8526623

Contents

SummaryDetails

Associated Components

Manufacturing General