Solid Edge Set SEEC BOM expansion "Level by Level" as default

2021-10-06T23:58:07Z
DOC_MANAGEMENT

Summary


Details

In this scenario the Customer has a massive assembly (for example, more than 10,000 unique files) with some draft files attached. 

In SEEC the only option to open this structure is by using the "level by level"  BOM expansion.  With the default option "optimal performance BOM expansion" it will fail.  The customer needs an option to set the level by level BOM expansion as default. 

How can we set BOM expansion by default to "level by Level" ?

Solution

We have a preference to expand the BOM level by level - this is "SEEC_ExpandStructure".  By setting the preference to 1 this will download the large assemblies level by level.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221MP3
Function: SEEC

Ref: 002-8526620

KB Article ID# PL8526620

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC