Can't display Teamcenter folder as Palette

2023-02-06T20:40:49Z

Summary


Details

When specifying a Teamcenter folder as a Palette in NX, the following message is displayed:

=============
Palette
Could not create the specified palette.
The specified folder could not be found.
<<OK>>
=============

Solution

1. In NX, select 'Preferences-->Palettes'.

2. Select the 'Open Folder as Palette' icon.

3. The format to specify an existing folder is:

<teamcenter_user>:<foldername_under_home>

For Example:   infodba:My_Files

If you still receive the message, make sure the folder name in Teamcenter does not have a invisible space after the name, or even a <return> after the name to an empty line. This can be checked by going to the Folder Properties in Teamcenter and looking at the 'Name' field.

Notes

KB Article ID# PL8526462

Contents

SummaryDetails

Associated Components