Details
LOV's attached to the attributes/properties are not available as a drop-down list on the "Save As New Item Type" main dialog.
Solution
LOV's attached to the attributes/properties are not available as drop-down lists in the "Save As New Item type" main dialog.
This is the existing behavior.
The user has to select the "Attributes" dialog on the main dialog, to select the drop-down lists of the attributes/properties.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1953
Function: FILE_SAVE_AS
Ref: 002-8526333