High processing consumption when working with SEWHD

2021-10-06T23:58:06Z

Summary


Details

Working with Solid Edge Electrical Design (SEWHD) and then opening the Task Administrator the processing consumed is so high (more than 50%), and when working, in some processes the software is locked and closed. In the picture below you can see a screen capture:

How to solve this to allow working .

Solution

Please use the following instructions to modify the "shortcut" that launches SEWHD.
 
·         Place your cursor in the Target field shown below.
·         Move your cursor to the end of the line.
·         Move your cursor to the left one increment.


Add in the memory argument of –Xmx2048m
This should help with overall speed and stability.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V221MP2
Function: OTHER

Ref: 002-8526238

KB Article ID# PL8526238

Contents

SummaryDetails

Associated Components