NX Convert Tool Library fails with "No type or subtype field found"

2021-10-06T23:27:53Z
NX for Manufacturing

Summary


Details

Menu -> Tools -> Convert Tool Library

Gives error message :  "No type or subtype field found"



Solution

This error will be given if the user attempts to convert the 'holder_database.dat' file

Note that the 'Convert Tool Library' should NOT be done on the 'holder_database.dat' file. It should ONLY be done on the 'rtool_database.dat' file.  The  'holder_database.dat' will then be automatically converted if necessary.

Reference NX Help documentation:


https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200507135732916.mfggeneral/html/converting_tool_lib

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: NX
Application: CAM
Version: V1957
Function: LIBRARIES

Ref: 002-8526146

KB Article ID# PL8526146

Contents

SummaryDetails

Associated Components

Manufacturing General