Editing the format of Annotation created using the 'Measure' command requires a PMI license...

2021-10-06T23:27:52Z

Summary


Details

Editing the appearance/format of Annotation created using the 'Measure' command requires a PMI ('geometric_tol') license.


In NX 1899 (December 2019 Functional Release) and later, it is not possible to select annotation in the  Modeling application and access the 'Settings' command (via right-hand mouse button), if no PMI 'geometric_tol' license feature is available. (No error message is displayed, the 'Settings' command is simply not displayed.) This limitation applies to annotation created using the 'Measure' command and/or the PMI application.

The 'Menu - Edit - Settings' command is also greyed-out.

In NX 1872 Series (and earlier), it was possible to edit the appearance/format of 3D annotation, via 'Settings', without the need for a PMI ('geometric_tol') license. 



Solution

This issue is scheduled to be fixed in the NX 1980 - June 2021 Functional Release.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1899
Function: INFO_ANALYSIS

Ref: 001-8468321

KB Article ID# PL8525975

Contents

SummaryDetails

Associated Components