NX Text added in thread size field is not visible in Thread callout

2021-10-06T23:27:52Z
NX for Design

Summary


Details

Is it possible to add customer hole sizes(Custom)?

In the thread table, we defined wire coil thread like below.
But, when we add PMI Hole and Thread callout, "Wire coil" text is missing in size.





Solution

Yes, the XML file can be modified and the callout section in the XML file can get the name of the thread in the dropdown.

Please make modifications to the XML file as shown below in the Callout section.
This should enable you to display the required notations in the PMI.


Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1909
Product: NX
Application: DESIGN
Version: V1934
Function: FEATURE_MODEL

Ref: 001-9980297

KB Article ID# PL8525532

Contents

SummaryDetails

Associated Components

Modeling