Subassembly components not displayed in higher level assembly

2021-10-06T23:27:52Z

Summary


Details

After adding a sub-assembly to a higher level assembly, none of the sub-assembly components display in the work area.

Solution

After adding the sub-assembly to the higher level assembly verify the reference set in the sub-assembly.
1.  Verify the higher level assembly is the Work Part and expand the Assembly Navigator.
2. Highlight the Sub-assembly and right click on it.
3. Select Replace Reference Set.
4. Set it to Entire Part.
5. The components of the sub-assembly will now be displayed in the work area.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V12.0.2
Function: ASSEMBLY_MODEL

Ref: 002-8525528

KB Article ID# PL8525528

Contents

SummaryDetails

Associated Components