Patch RealNC 8.7.0.204 is available

2021-10-07T00:16:42Z

Summary


Details

Dear Siemens Digital Industries Software Customer,
                                                                               
We are pleased to inform you that the patch "RealNC V8.7.0.204" is available for download from:
           https://support.sw.siemens.com/

Please select "Tecnomatix Legacy" at "My products".
Click on "Downloads".
Select version "RealNC 8" and click on "RealNC 8.7_Patches"

There you will find the zip-files:
RealNC_8.7.0_Patch_204_32bit.zip
RealNC_8.7.0_Patch_204_64bit.zip
and the RealNC_8.7_Hotfix_Master_List.xls for details concerning the patches.
                                                                               
Assuming that the symbolic name $RealNC$ is the full path to your RealNC installation and
$Version$ is the version e.g. v8.7

Download the needed zip-file (depending on your installation either 32bit or 64bit) and put them into a folder ($RealNC$/downloads is suggested).
Extract the zip-file content into $RealNC$/$Version$/bin.
                                                                               
The default for RealNC (32bit) is:
              C:\Program Files (x86)\Tecnomatix\RealNC.
                                                                         
The default for RealNC (64bit) is:
              C:\Program Files\Tecnomatix\RealNC.
               
This patch also includes an update of the file "CSE Documentation.chm".
If you have a MachineConfigurator installed please update the file in you installation with the version included.
           
If you have any issues with the installation or support of these fixes, please contact your local GTAC support group.

Sincerely,
                                                                                
Siemens Digital Industries Software 

SFB-TECNOMATIX-8525527
PR 9586318, 9837629, 9772954
Product Information:
  • Product: TECNOMATIX , Application: REALNC , Version: V8.7.X

KB Article ID# PL8525527

Contents

SummaryDetails

Associated Components