How to create a dimension in NX Drafting with a double arrowhead terminating at a distant point?
2021-10-06T23:27:52Z
Summary
Details
How to create a dimension in a Drafting Detail View that has a double arrowhead, to indicate that the dimension terminates at a distant point?
Solution
1. Create a Detail View on the Drawing
2. Create a Linear dimension by selecting the first object in the Detail View and the second object in an Orthogonal View:3. Select the dimension with the right-hand mouse button and choose 'Settings'. Within the Settings dialog select 'Single Sided' and check the 'Display as Single Sided Dimension' option (select the 'Flip Dimension Side' icon, if required:4. In the 'Settings' dialog, select 'Line/Arrow - Arrowhead' and change the 'Dimension Side 2 - Type' from 'None' to 'Filled Double Arrow', 'Close':
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DRAFTING Version: V12.0.2 Function: DIMENSION