Simcenter 3D Solutions About the part attribute "Material".

2021-10-06T23:27:52Z
Simcenter 3D

Summary


Details

Legacy part files (pre NX8), have the attribute "Material" set to "Not Defined" (originates from our template parts). 

This has worked fine for quite some time but, now in NX12 or higher version, when we open a legacy part file or add it as a component, we always get an information window with the statement: 

"The Material Attribute was reset because it did not match the material assignment. 

This action was taken based on your Customer Default setting." 

Solution

The message highlights that the Material attribute in the part file being opened has a value set that is NOT related to a material assigned to a solid body and subsequently there are necessarily no physical properties defined for the solid body. 

The attribute defined in NX Customer Defaults Gateway --> Materials/Mass, Attributes tab, Part Material group, Attribute Title Alias field, is an NX system attribute which is reserved to be used by NX to store the material name defined when using Assign Material function. 

In earlier versions, there was no check or prevention to manually set this attribute. Now if a part file is opened with the "Material" attribute value set manually, the "Material" attribute WILL BE REMOVED. 

To avoid such situations:

  • Ensure to have the material assigned to the solid body and is picked from either system library(OOTB) or a Natively defined local library.

    Notes

    9959408

    KB Article ID# PL8525327

    Contents

    SummaryDetails

    Associated Components

    Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow