NX
Can't use a Feature Group as parent geometry to a Zlevel Profile operation
2021-10-06T23:27:52Z
NX for Manufacturing
Summary
Details
When creating a Zlevel Profile operation, it is not possible to select an existing Feature Group as the parent geometry.
How can such an operation be added beneath a Feature Group?
Solution
Currently it is not possible to use a Feature Group as a direct parent geometry to Planar Milling or Zlevel Milling operations. A Mill Boundary or Mill Area geometry object must be used in between.
In the use case above, a Mill Area object should be created under the Feature Group. Then the Zlevel Profile operation can be created, using the Mill Area geometry as parent.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: CAM Version: V1953 Function: FEATURE_BASED